Communication between AEK-COM-ISOSPI and AEK-MCU-C1MLIT1 boards
Good morning!
I've been working in a project whose purpose is communicate AEK-MCU-C1MLIT1 board and AEK-COM-ISOSPI1 through SPI/isoSPI protocols. At first, I've tried to apply the hardware configurations and script as mentioned in the user manual(UM3187) to exchange 512 bytes between two devices through isoSPI, however I don’t know how reliable the results in debug step are to assure this communication is working properly. Another detail that I've noticed is about disable pin, which stay always turned on, mainly when I select configuration as “micro” in AEK-COM-ISOSPI1 Component RLA > Application Cofiguration. What should I do to enable AEK-COM-ISOSPI1 board?
About the wire connections, I used as reference the board view within AutoDevKit Studio. I’d like to know if there is some connection that is missing, especially about the ISOm e ISOp signals, because the board view doesn’t show if I should to connect the USB port on the computer to debug step, for instance.
Debug step:


Board View within AutoDevKit Studio

Thank you!