Skip to main content
Associate III
May 22, 2024
Solved

How to add extra memory to the AEK-AUDC1D9031 board

  • May 22, 2024
  • 1 reply
  • 1856 views

hi 

1. on AEK-AUDC1D9031 there is SPC582B60E1 MCU with 1 Mb flash.

2. i want to more wav files to play. but SPC582B60E1 is has only 1MB.

3. so that i want to know how to integrate the extra memory to the  AEK-AUDC1D9031 board.

4. how to connect external memory and flash that memory and how to PLAY sound files with respective to the external memory.

Best answer by Max VIZZINI

Hi,

Excluding the EEPROM, the MCU SPC582B has no other direct memory interface because RAM and FLASH are embedded in the package.

If you change to other SPC58 MCU ( SPC584B  - 2 MB flash / SPC58EC - 4 MB flash ), you do not need to change the source code as it is compatible.

A third alternative to be tested is to use external memories coming from Mass Storage (e.g. Memory card via SPI) or from other MCU (e.g. via CAN). These implementations are not included in our code.

 

Best Regards,

AutoDevKit Team

1 reply

Max VIZZINI
Technical Moderator
May 22, 2024

Hi,

If you need extra FLASH you can consider the following alternative micros:

SPC584B  - 2 MB flash

SPC58EC - 4 MB flash

Best Regards,

AutoDevKit Team

Associate III
May 23, 2024

hi 

     actually i am using AEK-AUDC1D9031 PCB board with SPC582B60E1. hear the MC is fixed for this i want to include the external memory. without changing the MC. so please suggest the alternative solution to include external memory .

shiva_shankar_e_0-1716432402350.png