How to read initialization from L9663 data using SPI?
Hello,
I stareted to develop PSI5 interface with L9663. My point is to read initialization data via SPI. If I set DOUT1 as direct data output (CH1_CR1->DOUT1_SE = 0), I am able to measure received data on this pin. But if I set this pin as interrupt (CH1_CR1->DOUT1_SE = 1), then I am not able to read initialization data via SPI (but interrupt is active).
My procedure:
1. set READ_INIT_DATA1 bit in CH1_CR1
2. Enable PSI5 (with requierd settings)
3. Reading initialization data by this command:

After this INITDATA_RDY in SR3 is not set. Is this procedure correct? What I should write to "init_buf_id" and "Register" bits? I tried to make loop for all possible combinations, but there wasn't any data.
Thank you for your response.