Motor Control using STEVAL-TTM001V1 kit and STEVAL -TTM002V1 CONTROLLER using SPC5 Studio example application not working
Hi
We are using STEVAL -TTM001V1 Kit which consists of L9907 driver and trying to interface it with STEVAL-TTM002V1 Controller board (SPC560P50L3) to run the O-Drive 5312 Motor.
We are using the sample program SPC560P50L3_MotorControl_STEVAL-TTM001V1 from application library to run the motor.

We have changed the motor parameters according to O-Drive 5312 motor in the motor settings of the motor control component.

Then generated the application code in Observer + PLL ( Sensorless ) mode to run the motor. We are not getting any waveform in the PWM pin when checked with an oscilloscope.
- We tried to debug the code generated but the variables are showing not found.
- We also tried by enabling the Demo Mode but still it doesn't work.
- Do we need to set anything other than motor parameters ?
Are we missing out anything else ?