Skip to main content
ssk
Associate III
March 19, 2015
Question

Application Configuration - ISRs - Headers

  • March 19, 2015
  • 16 replies
  • 2183 views
Posted on March 19, 2015 at 11:59

I have configured few interrupts using Application Configuration -> ISRs (under SPC OSAL Component). I have multiple header files which I supplied to the 'Headers' parameter under 'ISRs'. I have provided 4 different header files. For another interrupt, I want one more header file. When I try to add one more file i.e. 5th one, the SPC5Studio IDE hangs (initially shows busy but later changes to 'not responding' and can not be exited). Is ther limit for no of header files for ISRs? Why is this issue?

Thanks.

Mike.

#interrupts---headers
    This topic has been closed for replies.

    16 replies

    Nickname2551_O
    Visitor II
    March 31, 2015
    Posted on March 31, 2015 at 15:52

    Hello Mike,

    the errors you mentionned are to be considered as warnings, and are not related to this topic.

    As soon as the version SPC5Studio3.4.3 has been delivered today (including the fixes related to this thread), let's consider this ticket as solved.

    Thanks and regards

    Philippe 

    ssk
    sskAuthor
    Associate III
    April 1, 2015
    Posted on April 01, 2015 at 07:40

    Thanks Philippe. Few errors have been converted to warnings but still errors are there. Not sure how harmful it is for the code. Please see attached error logs.

    Thanks.

    Mike.

    ________________

    Attachments :

    SPC_ErrorLog_v3_4_2.log : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hta1&d=%2Fa%2F0X0000000aRz%2FDdUvVPhtoP3Etub.UJ5OMZw.buWBSIt50KS9iJH6yx0&asPdf=false

    SPC_ErrorLog_v3_4_3.log : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtYk&d=%2Fa%2F0X0000000aRl%2FTyq0EY02bKubbwDMU2JgksfmOpTvllA07D73C5H0roc&asPdf=false
    Nickname2551_O
    Visitor II
    April 1, 2015
    Posted on April 01, 2015 at 09:17

    Hello Mike,

    do you have any systematic step by step way of reproducing the problem ?

    I can see in the logs some ''Invalid Thread access'' that we did not observe on our side.

    Regards

    Philippe

    ssk
    sskAuthor
    Associate III
    April 1, 2015
    Posted on April 01, 2015 at 14:39

    Hello Philippe,

    I am cleaning my existing project and building it again. When I clean the project it displays these error log. Similarly, when I try to Generate Application, then also it displays the same. Other than this I am doing nothing.

    BTW, What is the cause for this? I haven't seen this earlier for similar actions as said above.

    Thanks.

    Mike.

    Erwan YVIN
    ST Employee
    April 2, 2015
    Posted on April 02, 2015 at 11:22

    Hello Mike ,

    Could you confirm your Hardware used ?

    Processor, RAM , OS (Windows 7 (32Bits ? 64 Bits ?), Windows 8), Language Pack.

    We will try to reproduce with a Virtual Machine .

    Best Regards

                         Erwan

    ssk
    sskAuthor
    Associate III
    April 3, 2015
    Posted on April 03, 2015 at 07:39

    Hello Erwan,

    Please find attached image for the below information. The language is English (US) only. No other packs installed.

    Thanks.

    Mike.

    ________________

    Attachments :

    ST_SPC_ISR_Headers_plugin_error_04.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtCE&d=%2Fa%2F0X0000000aKC%2FZgrezGgVYbCRFtv8U6B1gkd2tr9qeJKNavCaPP3xyMc&asPdf=false