Skip to main content
prashanth.mohan22
Associate III
September 25, 2019
Question

can't communicate with target processor

  • September 25, 2019
  • 2 replies
  • 1101 views

HI,

I'm having PEMicro USB-ML debugger and try connecting it with SPC560B-DIS board.

But I'm not able to connect with the target. I could able to see both target power and USB power glowing in the USB-ML hardware.

As well, I updated the PROGPPCNEXUS firmware. Still not resolved. Please help me over.

0690X000009jAmQQAU.png0690X000009jAmLQAU.png0690X000009jAmGQAU.jpg

Best Regards,

Prashanth Mohan

    This topic has been closed for replies.

    2 replies

    Erwan YVIN
    ST Employee
    September 25, 2019

    Hello ,

    Sorry,

    I have not PEMicro USB-ML debugger

    Have you checked the jumper settings of Table 3 chap 2.4 of UM1672 SPC560B-DIS discovery board

    Best regards

    Erwan

    prashanth.mohan22
    Associate III
    September 25, 2019

    HI @Erwan YVIN​ ,

    Thanks for your advice.

    I checked it, so, what I have to do with J19 & J20 (soldered jumpers) for connecting external debugger?

    if it is working for integrated debugger, no change in that jumper configuration should do fine, but it is not. So need help on this.

    0690X000009jBYKQA2.png

    Regards,

    Prashanth