Skip to main content
David_D
Associate II
September 17, 2021
Solved

Can't connect to target with UDE 5.0

  • September 17, 2021
  • 2 replies
  • 1701 views

Hi,

I am working with SPC58xx, SPC5Stuido 6.0, Windows 10 and I am trying to deploy the code onto the board with UDE 5.0.

Although I've read all the topics about these issues I still can't connect to target.

The drivers have been installed properly and the Load VCA settings are enabled.

What else can I do to make it work?

Thank you!

    This topic has been closed for replies.
    Best answer by David_D

    Issue has been resolved. Micro was fitted in the incorrect position.

    2 replies

    David_D
    David_DAuthor
    Associate II
    September 23, 2021

    I've installed UDE 5.2 and tried with that one and still doesn't work. The adapter board is SPC58xxDPT176S. The micro is SPC58EE48E7.

    The target configuration file is automatically selected in SPC5Studio 6.0 as SPC58NE84. Will this be a problem?

    David_D
    David_DAuthorBest answer
    Associate II
    September 29, 2021

    Issue has been resolved. Micro was fitted in the incorrect position.