Connect to eMoticom eM007 ECU
I have an eMoticom eM007 ECU on a motorcycle which has been developed from the SPC5-L9177A-K02 dev kit. I wish to connect to the ECU to download the bin file so I can learn to tune it. The ECU has a canbus connector with 4 pins +12v, Gnd, CAN-H, and CAN-L. I have purchased the ST-Link-V3MODS board with the view of using the bridge CAN interface to connect to the ECU. How should this be connected as the Bridge CAN only has logic signals Rx/Tx using pins 9 and 10 on CN2. Any help will be appreciated as I don't want to brick the ECU on connection.
Will I be able to use the STM32CubeProgrammer to download the bin file from the ECU and re-flash it once the edits to the tune have been done. Also will it be possible to write on the fly.