GCC compile and flash code
Is it possible to compile the application only with Gcc (free) so do not use GHS or Hightec and flash and run the compiled code?
I can tolerate that this compiler is not efficient as those not free.
Is it possible to compile the application only with Gcc (free) so do not use GHS or Hightec and flash and run the compiled code?
I can tolerate that this compiler is not efficient as those not free.
Yes , it is possible for you to use gcc (free) for SPC5 Family
The compiler is available on the update site (SPC5Studio Update site)
http://spc5tools.spc5studio.com
you should download from SPC5Studio Tools suite
Best regards
Erwan
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.