Skip to main content
FErma
Associate II
October 7, 2019
Solved

Help for automotive grade mcu selection

  • October 7, 2019
  • 1 reply
  • 829 views

Hi everybody,

We are currently working on a commercial project for automotive industry. Since we are used to use ST mcus, we want to continue ST's automotive grade mcu. The requirements are listed below;

- AEC-Q100 compliant

- ASILB or higher level qualification.

- At least 2xCAN peripheral

- RTC timer

- External 32 khz connection option

- At least 1 x I2C

The mcu which almost meets that requirements I found is SPC560b50l3 but I am not sure if it is compliant with AEC-Q100 and ASILB or higher qualification. Can you please confirm or recommend another ST mcu?

Thanks in advance 

    This topic has been closed for replies.
    Best answer by Erwan YVIN

    Hello ,

    SPC560B50L3 is AEC-Q100 qualification compliant

    For ASILB , you should use 58 family or 56L

    cf link

    https://www.st.com/en/automotive-microcontrollers/spc5-p-performance-mcus.html

    Best regards

    Erwan

    1 reply

    Erwan YVIN
    Erwan YVINBest answer
    ST Employee
    October 31, 2019

    Hello ,

    SPC560B50L3 is AEC-Q100 qualification compliant

    For ASILB , you should use 58 family or 56L

    cf link

    https://www.st.com/en/automotive-microcontrollers/spc5-p-performance-mcus.html

    Best regards

    Erwan