Solved
How CAN Filter Work on Pictus
Posted on February 17, 2015 at 15:46
I am testing CAN filtering Function on SPC560P,But am not clear about how CAN Mask working.
Configure as following: Rx ID =0, Rx Individual Mask = 0xFFFFFF8; BCC = 1; From my understanding, then the CAN Node can Receive ID from 0 to 7, but cannot , only still can receive ID = 0; stop at BUF00 Rx Flag checked; But , when I set Rx Individual Mask = 0; all CAN ID can be received (stop at BUF00 Rx Flag checked); So, How the CAN ID Mask Working? ----------------- CAN_0.RXIMR[0].R = 0xFFFFFFF8; /*Rx Individual Mask*/ CAN_0.BUF[0].ID.B.STD_ID = 0x0; /*Rx ID = 0*/ /*Check ID Receive*/if(1== CAN_0.IFRL.B.BUF00I){
CAN_0.IFRL.B.BUF00I = 1; // rx completed}