How do I proceed a wakeup on SPC584Cx/SPC58ECx 32-bit MCU Chorus 4M?
Hello everybody,
My name is Catalin and I work on an Automotive project on a gateway and I have a question regarding this microcontroler.
So basically I have to wakeup the gateway every 600 seconds +/- 15 seconds and perform a voltage measurement. As I read in the reference manual there is this RTC_APIVAL register which its bits are compared to the RTC counter bits and if a match occurs, an wakeup request is asserted. I tried in so many ways to make that work but I didn't manage to do it.
Here is my code so far:
void rtc_init(void)
{
/*Disable Real Timer Counter Module for initialization*/
RTC_API.RTCC.B.CNTEN = 0u;
PMCDIG.MISC_CTRL_REG.B.SIRC_ENB = 0; // Enable SIRC in running modes
RC128K_DIG.CTL.B.LPRCON_STDBY = 1; // Enable SIRC in STANDBY
/*select clock SIRC 128 KHz*/
RTC_API.RTCC.B.CLKSEL = 1u;
/*enable divider by 32*/
RTC_API.RTCC.B.DIV32EN = 1u;
/*disable divider by 512*/
RTC_API.RTCC.B.DIV512EN = 0u;
RTC_API.RTCC.B.APIEN = 0;
RTC_API.RTC_APIVAL.B.APIVAL = 2400000; // API period 1/4000Hz * 2400000= 600sec?
RTC_API.RTCC.R = 0x80009001; //Counter enabled, API enabled, SIRC@128KHz used, Trigger enabled for Analog Comparator Block
}And this is how I call it:
{
...
WKPU.WISR.R = 0x0002u; // clear possible RTC
rtc_init();
RTC_API.RTCS.R = 0x200002400; // Clear RTC flags
...
}Can you have a look at this code? It doesn't seem to work but I build it based on the reference manual.
Maybe the value of the APIVAL(2400000) is not good(It's not 600 seconds)?
Thank you. Best regards,
Catalin