Skip to main content
aurelien23
Associate III
June 26, 2015
Question

How to change mcuconf.h values in the code generator?

  • June 26, 2015
  • 2 replies
  • 672 views
Posted on June 26, 2015 at 15:34

Hello,

I always have to manually change some values in mcuconf.h when I generate the code out of the config because I can't find how to set them in the config or anywhere else.

I'm using a 16MHz external xtal and I have to set SPC5_FMPLL0_IDF_VALUE and SPC5_FMPLL1_IDF_VALUE to 2 instead of the default 5. Same for SPC5_MCONTROL_DIVIDER_VALUE that I have to set to 15 instead of 1 to get my ICU-PWM config to work. Where can I set these value in the config to get correct values on code generation?

Thank you for all improvments since the v2.0
    This topic has been closed for replies.

    2 replies

    Erwan YVIN
    ST Employee
    June 26, 2015
    Posted on June 26, 2015 at 16:27

    hello Aurelien ,

    mcuconf.h is generated from the configuration file.

    HAL Drivers ==> Initialisation settings ==> FMPLL0 Settings 

    Best regards

                     Erwan

    aurelien23
    Associate III
    June 29, 2015
    Posted on June 29, 2015 at 08:53

    Hello,

    Oops, I never noticed it was collapsed...

    Thank you!