Skip to main content
SIBIN THOMAS
Associate II
February 16, 2018
Question

How to check stack and heap usage during run time.

  • February 16, 2018
  • 3 replies
  • 5958 views
Posted on February 16, 2018 at 06:03

Hello Everyone,

I am working on SPC560C50L3 MCU with SPC5 Studio. I am trying to add a library file which uses heavy stack and heap using dynamic allocations into my application. My code used to stuck in between due to stack overflow. Now I am able to change the stack size in the user.ld file. But how do I check the stack and heap usage at run time ? Any suggestion would be helpful.

Regards

THOMAS.

#spc560 #stack-overflow
    This topic has been closed for replies.

    3 replies

    Tesla DeLorean
    Guru
    February 16, 2018
    Posted on February 16, 2018 at 07:27

    Don't have specific experience with the SPC5 but the typical way to figure stack depth is to fill it with a pattern you can recognize later, and then periodically measure the low-water mark (see how much of the pattern remains walking up from the bottom of the stack's allocation). For heap, wrap the malloc/free to instrument, or write a routine to walk the allocator's structures in the memory arena. ie understand how your allocator manages its space.

    If you don't know who's taking the memory, or leaking resources, then you'd want malloc() to tag the allocations so you know. For example use the return address of the malloc caller, and then associate with map or symbol file.

    Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
    Bogdan Golab
    Lead
    February 17, 2018
    Posted on February 17, 2018 at 21:23

    I was really interested what is the current solution for the stack monitoring. The 0xDEADBEEF pattern approach was taught in 80ties when I was in the electronic-oriented school.

    I am happy that the approach is still used.

    Tesla DeLorean
    Guru
    February 18, 2018
    Posted on February 18, 2018 at 16:05

    Well I did travel here from the 80's so not exactly surprising. You tended to be resourceful because an ICE would cost as much as a car, and while trace/profile pods are now much cheaper a lot of people don't have them, or header connections to support them.

    Some tools provide for static analysis of call trees and stack depth, but interrupts and nesting there tends to be a bigger unknown factor.

    Most things I build have a command line monitor to permit field debug/analysis, these typically include a reporting of stack depth as perceived from the console, and after running test/diagnostic routines. Also try to provide a register dump in case of hard failure, so we have something to work from than trying to determine the flashing pattern of an LED, or silent death. Hot-plugging a system isn't always practical or reliable.

    Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
    Erwan YVIN
    ST Employee
    February 16, 2018
    Posted on February 16, 2018 at 10:09

    Hello Thomas ,

    • if you want to update a SPC5Studio demo, you can update this following configuration , save and generate
    0690X00000609eAQAQ.png
    • If you want to use your own linker file

            in SPC5Studio, rename application.ld by user.ld

    and you can customize your stack size by updating this following value

    0690X00000609i1QAA.png

                 Best Regards

                                Erwan

    SIBIN THOMAS
    Associate II
    February 16, 2018
    Posted on February 16, 2018 at 16:58

    Hello,

    Yes, i am able to change my stack size in the user.ld file. But my ultimate aim is to calculate the stack and heap usage during run time and if they exceeds a certain value, i have to do a soft reset to recover leaked memory. So is there any way to keep track of my stack and heap usage while the code is running.

    'Filling the stack with a pattern' is this the only way or is there any current stack pointer for checking the stack usage ?

    For heap usage, how do I use my malloc/free to keep track of the remaining free space ?

    Regards

    Thomas.

    Tesla DeLorean
    Guru
    February 16, 2018
    Posted on February 16, 2018 at 17:51

    You could record the deepest stack pointer value seen under a periodic interrupt, 1ms ticker if you have one.

    For malloc/free, perhaps understand how the heap actually works on your platform, wrap the routine, allocate slightly more memory so you can place a variable/structure in front, and advance the pointer returned to the user, reverse that on the free, and perhaps count malloc/free calls to see if they balance, or if you free the same memory twice, etc.

    Review source or disassembly of allocator currently in use, likely to use a simple linked list, figure how to walk.

    Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..