Skip to main content
PSing.5
Associate II
July 22, 2021
Solved

How to get double wire CAN from SPC5?

  • July 22, 2021
  • 1 reply
  • 771 views

SPC5Studio asks for a TX and RX pin. I selected CAN 1 TX and RX pins and connected them to CAN 2 RX and TX pins I chose (I tried all manner of connections). I am trying to get CAN 2 to send a message. On the output I see a 0 to 5 V signal instead of 0 to 2.5 V and another of 2.5 to 5 V. How do I get two wire CAN? I think I am missing a concept here, can someone please help me.

I am trying to use SPC560B discovery board.

    This topic has been closed for replies.
    Best answer by PSing.5

    To anyone reading this in the future, the answer to my question was the SPC56 DIS board does not come with a transceiver to produce a CAN_H and CAN_L.

    1 reply

    PSing.5
    PSing.5AuthorBest answer
    Associate II
    July 23, 2021

    To anyone reading this in the future, the answer to my question was the SPC56 DIS board does not come with a transceiver to produce a CAN_H and CAN_L.