Skip to main content
RSeba.2
Associate III
December 8, 2022
Question

I am configuring the flexray controller. For PE clock I configured XOSC oscillator in FR_MCR register. However, to enable XOSC, we need to enable XOSC_EN in Miscellaneous DCF registers, as I read from the documentation. How can I do it ? Also, CHI fr

  • December 8, 2022
  • 1 reply
  • 780 views

..

This topic has been closed for replies.

1 reply

GCOND.1
Visitor II
December 12, 2022

Hello,

XOSC_EN bit in Miscellaneous DCF helps for enabling the oscillator at device startup and the default configuration is with XOSC OFF. In your case I think you are just in one of the running modes the device supports. This is the common scenario and you have to enable the XOSC via the Mode Entry Module (MC_ME). Please refer to the dedicated chapter in the Reference Manuals for the correct procedure.

Best Regards,

Giuseppe