Skip to main content
Sk1
Visitor II
January 29, 2020
Question

I wanted to know JTAG PIN details of the SPC5-UDESTK-PLUS Debugger

  • January 29, 2020
  • 1 reply
  • 664 views

Hi All,

I am unable to connect target to the UDE.

1)Is there any necessity to install virtual Com port drivers for debugging with UDE-STK-PLUS debugger apart from the drivers provided by the UDE software ?

2) How to integrate SPC5 studio with UDE-STK-PLUS ?

3) Also, please share  JTAG PIN details of the SPC5-UDESTK-PLUS Debugger. So that I can verify the target connection with UDE-STK-PLUS.

Thanks in advance.

    This topic has been closed for replies.

    1 reply

    Erwan YVIN
    ST Employee
    January 30, 2020

    Hello Sk ,

    1) No, Virtual Com Port drivers are only useful to use Serial Port (using printf mecanism)

    2) There are "UDE Eclipse 4 integration" in http://spc5tools.spc5studio.com/

    you can install it

    but PLS UDE should be installed in your PC

    3) Which board do you use ? i think that the information is in the datasheet

    Best Regards

    Erwan