Skip to main content
CCOLL.2
Associate II
September 15, 2022
Solved

If I use SPC5 studio, do I need to be on a STM discovery kip or evaluation board to be able to flash and debug a board with a SPC582B or SPC584B MCU (I have also a probe SPC5-UDESTK) ?

  • September 15, 2022
  • 4 replies
  • 2188 views

Hi,

I'm new in SPC5 world.

I would like to use SPC5-Studio to start my project on a SPC582B product and I would like to be able to debug it.

I have a probe SPC5-UDESTK that I have used to flash a project compiled with SPC5-Studio.

It is not clear if I need to by some licences or if I can continue with free licence.

I have also read that the debug purposes of SPC5-studio is only available on STM development kits. Is-it the case ?

Do I need to use PLS UDE STK tool to debug a project or, is-it possible using SPC5-studio directly ? do I need to buy a new licence in order to debug ?

Thanks,

Christophe

    This topic has been closed for replies.
    Best answer by Erwan YVIN

    Hello,

    for SPC582B-DIS , (Discovery Kit)

    https://www.st.com/en/evaluation-tools/spc582b-dis.html

    you do need SPC5-UDESTK just a USB Mini cable is enough to flash and debug

    for SPC582B (Motherboard and Mini-Module)

    you need SPC5-UDESTK and USB Mini cable

    It includes a perpetual, full-feature, limited code-size (256 kBytes) license. (Flash and debug)

    it is often enough for projects

    Best Regards

    Erwan

    4 replies

    Erwan YVIN
    Erwan YVINBest answer
    ST Employee
    September 16, 2022

    Hello,

    for SPC582B-DIS , (Discovery Kit)

    https://www.st.com/en/evaluation-tools/spc582b-dis.html

    you do need SPC5-UDESTK just a USB Mini cable is enough to flash and debug

    for SPC582B (Motherboard and Mini-Module)

    you need SPC5-UDESTK and USB Mini cable

    It includes a perpetual, full-feature, limited code-size (256 kBytes) license. (Flash and debug)

    it is often enough for projects

    Best Regards

    Erwan

    CCOLL.2
    CCOLL.2Author
    Associate II
    September 16, 2022

    Hi,

    Thanks for your answer.

    But, if I do not use a STM board (I have a prototype done by a customer), is SPC5 studio able to debug on it ?

    We plan to make a new project based on the same SPC582B or 4B chip and I would like to use this board to work on it during the pre-study.

    Rgds,

    Christophe

    Erwan YVIN
    ST Employee
    September 16, 2022

    Hello Christophe ,

    I hope that the JTAG port is well present and well plugged in your prototype board.

    SPC5-UDESTK could be plugged.

    Anyway , SPC5 Studio is eclipse based.

    It is possible to install to additional plugins (TRACE32,PLS UDE or others compliant for PPC VLE e200z) , debug and flash.

    Best Regards

    Erwan

    CCOLL.2
    CCOLL.2Author
    Associate II
    September 16, 2022

    Hi,

    Yes, on the previous project, JTAG was used to flash the board only so, I assume that it is physicaly OK.

    Thanks for the info about plugins, I have just installed the UDE plugin.

    I will check how many signals are available in the JTAG interface but, as we have already a trace32 probe (even if I suppose that we need a specific interface for SPC5), it could be interresting to use it during this pre-study.

    Rgds,

    Christophe

    jmary
    Associate III
    September 17, 2022

    Hi, I create spc5-udestk from the SPC574 discovery board schematic.

    Anyone willing to send me the ude memtool flash programmer?