Importing SPC5Studio V3.5 project using V5.0
Hi,
I need to work on old project created using SPC5Studio V3.5. Project is created using Wizards. When I open same project using V5.0, the 'Configuration.xml' is showing some error (red cross against file name). If I try to generate new code using 'Configuration.xml' it is giving following error messages
hal_lld.h 1.0.0.201609071703 : ...CAN NOT APPLY THE PATCH...
FlashMap.h 1.0.0.201609061636 : ...CAN NOT APPLY THE PATCH...
Am I doing something wrong?
First time I am using SPC5Studio