Question
Interrupt vector number
Posted on February 18, 2015 at 14:22
Hello Members,
I am using SPC560D030 for a product. I have connected PE0 and PB1 to use as wakeup. I want to have system wakeup functionality based on CAN request received (PB1) or when a +5V is applied to a pin PE0. When I try to configure these pins for wakeup using SPC5Studio, it asks for the ISR vector number. I tried assigning number 46 for both the interrupts but it generates an error. As per the reference manual (CD00259063.pdf) table 143: Interrupt Vector Table, these two interrupts fall under WakeUp_IRQ_0 having IRQ ♯ as 46. It looks like my understanding is incorrect for IRQ and ISR vector number. How can I identify the correct ISR vector number for the required wakeup signal? This I want for external interrupt as well.Thanks in advance for your help.Mike. #vector-number