Skip to main content
tga
Visitor II
September 18, 2020
Solved

PLS eclipse integration not working in SPC5Studio asimov

  • September 18, 2020
  • 1 reply
  • 856 views

Hello!

I am desperately trying to get the PLS integration to work but it is failing in every regard. When trying to create a "Universal Debug Engine" Debug Configuration, I am greeted with this:

0693W000004GOR4QAO.png

I do have all recent updates applied in SPC5Studio.

If I try to "Launch UDE Debugger on SPC5 Application":

0693W000004GOWYQA4.png

I am greeted with this:

0693W000004GOXHQA4.png

...no indication of any error, neither in Console nor in Problems view.

    This topic has been closed for replies.
    Best answer by Erwan YVIN

    Hello ,

    UDE Plugins is developed by PLS.

    "The current SPC5-UDESTK version 5.0.x is a 32Bit application.

    It is not compatible using 64Bit eclipse. It will not work with 64Bit Eclipse.

    The upcoming SPC5-UDESTK 5.2.x is a 32Bit as well.

    A 64Bit version of UDE and SPC5-UDESTK is planned but will be available not before Q1/2021."

    Best regards

    Erwan

    1 reply

    Erwan YVIN
    Erwan YVINBest answer
    ST Employee
    September 23, 2020

    Hello ,

    UDE Plugins is developed by PLS.

    "The current SPC5-UDESTK version 5.0.x is a 32Bit application.

    It is not compatible using 64Bit eclipse. It will not work with 64Bit Eclipse.

    The upcoming SPC5-UDESTK 5.2.x is a 32Bit as well.

    A 64Bit version of UDE and SPC5-UDESTK is planned but will be available not before Q1/2021."

    Best regards

    Erwan