Skip to main content
Visitor II
July 15, 2024
Solved

Problems with running application on SR6G7

  • July 15, 2024
  • 2 replies
  • 996 views

Hello,

I am trying to run Projects\System\SIUL2\siul2LedBlink from StellarSDK_4.0.0 on a SR6G7EVBC4000P_RevA board. The project was successfully build. 

To flash the board in RAM, I am using the last version of Lauterbach. When running, it seems that it can't break on main.

For testing purposes, I was running the sieve_ram_aarch32_arm_v8r_le.elf using the same Lauterbach script and the execution and breaking on main was done as expected. On a deeper investigation, I have found out that the .elf file form Lauterbach differs from the one build. Those differences can be seen below.

elf_comparison.png

Also, I have tried running an example from Lauterbach using the NVM, but I get the following error: 

image.png

 

Do you have any suggestions to run Projects\System\SIUL2\siul2LedBlink on the board? Also, to flash an application on NVM and fix the flash programming error.

 

Thanks in advance :grinning_face:

This topic has been closed for replies.
Best answer by FSPIL

Hello Andrei,

SR6 information is provided under NDA.
For any question, please contact local ST support, and do not post information/questions in this public forum.

Thank you.

 

Best regards,

Francesco

2 replies

Erwan YVIN
ST Employee
July 15, 2024

Hello , 

I am checking with Local FAE and SDK SR6

                         Best regards

                                     Erwan

 

              

FSPIL
FSPILBest answer
Technical Moderator
October 23, 2025

Hello Andrei,

SR6 information is provided under NDA.
For any question, please contact local ST support, and do not post information/questions in this public forum.

Thank you.

 

Best regards,

Francesco

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.