Skip to main content
Associate
November 21, 2025
Question

Request for Support – UART Bootloader Development for SPC582B60E1MH00Y MCU

  • November 21, 2025
  • 0 replies
  • 120 views

Dear Team,

 

@Max VIZZINI Sir, Help us to Solve this issue.

We are currently working with the SPC582B60E1MH00Y MCU in our project development. In our application, the ESP32 reads the firmware file from the cloud and sends it to the MCU via UART.

As part of our application, we need to implement a Bootloader using UART communication. However, we do not have prior experience with the Bootloader implementation on the SPC58 series MCU. The hardware design has already been completed, and the SPC58 UART is connected to the ESP32 through the LINFlex1 serial interface pins. Kindly confirm whether these UART pins can be used for the Bootloader application. 

We kindly request your support in developing the Bootloader application for our project. Additionally, if you could share any reference documents or sample projects (UART Bootloader code), it would greatly help us to progress further and improve our development status.

 

Our queries:

  1. How does the Bootloader work, and how can it be handled in the SPC582B MCU?
  2. Could you please share any sample project or reference code for a UART Bootloader?
  3. please confirm which file format should be used for the Bootloader application — .bin or .elf?

Thank you very much for your continuous support and guidance.

 

Best Regards,
Manikandaprabhu M.