Setting up program from scratch ?
Hey All
Fairy new to SPC5 development, coming from st's 32bit standard Micro controllers.
I have a few questions on the process to creating a project from scratch
1) Are we meant to just load the example projects and modify them according to our needs and add anything else OR can we start from scratch via New-> New spc project etcetc...
2)Starting a project from scratch, and adding in the SPC5Studio Pin map editor, i do what i would normal do in CubeMX, save, generate. but from that i just have the platform_component_rla file, and nothing more.
Referring to the help manual, under SPC5STUDIO -> Concepts -> spc5studio Projects
i'm missing my main components /dependencies. Is there a process to installing these into the project that i've missed ?

Here is a photo of my workspace.