Skip to main content
Erwan YVIN
ST Employee
December 21, 2017
Question

spc5.drive.cloudforge.com

  • December 21, 2017
  • 4 replies
  • 2507 views
Posted on December 21, 2017 at 11:04

SPC5Studio 5.7.1 is available

Dear All ,

SPC5Studio 5.7.1 is available

*** Highlights ***

Here are the changes coming with SPC5Studio v5.7.1

For Selected Customers:

================

- Network bugs fixing

Use these following update sites :

http://spc5.drive.cloudforge.com/projects/spc5releases/SPC5Studio/updates5

http://spc5.drive.cloudforge.com/projects/spc5tools/updates

(New update Site for free GCC feature and PLS Feature)

http://hightec.spc5studio.com/

(Hightec compiler)

                  Merry Christmas

                                 Erwan

#spc58 #spc5studio #spc56 #spc57
    This topic has been closed for replies.

    4 replies

    Guglielmo Spina
    Associate
    January 18, 2018
    Posted on January 18, 2018 at 12:23

    PinMap editor for SPC570S50 is available?

    Erwan YVIN
    ST Employee
    January 18, 2018
    Posted on January 18, 2018 at 15:11

    Yes , it is ;)

    Guglielmo Spina
    Associate
    February 1, 2018
    Posted on February 01, 2018 at 15:54

    it not working fine, because when I click on PinMap editor Link error message appears:

    'Device specific model 'SPC570S50E1' not supported!'

    Erwan YVIN
    ST Employee
    February 2, 2018
    Posted on February 02, 2018 at 10:25

    Yes , it is supported

    have you installed the last version of the pinmap  ?

    Cf SPC5Studio marketplace

               Best regards

                         Erwan

    Yalin Gurcan
    Associate III
    June 5, 2018
    Posted on June 05, 2018 at 16:05

    I have the latest version of pinmap installed from the marketplace but I still have the same problem. I'm using the SPC570S-DISP eval board.

    Patriks
    Senior
    February 11, 2018
    Posted on February 11, 2018 at 13:20

    Does SPC5 Studio support new SPC58x microcontrollers? If not is it planned to implemented support for theses controllers soon? I´ve installed the new SPC5 Studio release and would like to experience with SPC582B-DIS board.

    Erwan YVIN
    ST Employee
    February 12, 2018
    Posted on February 12, 2018 at 09:42

    Hello ,

    Please refer to the installation procedure after downloading SPC5Studio

    for SPC58x family ,it is for selected customers 

    could you send an email to

    mailto:credentials@spc5studio.com

     ?

    if the marketing guys are ok , we will send you a login/pass for spc58x support

      Best regards

           

                  Erwan