SPC560P ADC value not updating
Hello,
I am workin on SPC560P Discovery Board. I am trying to initialize the ADCperipheral using the components provided in the SPC5 Studio. What I am trying to do is to replicate the ADC Test Application in a different project. I initialize the ADC component in the project configuration andusing this in the main.c
#include 'components.h'
#include 'adc_lld_cfg.h'
static adcsample_t samples[ADC1_GROUP_ADC1_CONF_NUM_CHANNELS *
ADC1_GROUP_ADC1_CONF_BUF_DEPTH];
static uint32_t mswaittime;
int main(void) {
componentsInit();
irqIsrEnable();
adc_lld_start(&ADCD2, NULL);
sysWaitMilliseconds(1000UL);
while(1) {
adc_lld_start_conversion(&ADCD2, &adc1_group_ADC1_conf,
samples, ADC1_GROUP_ADC1_CONF_BUF_DEPTH);
mswaittime = samples[0];
sysWaitMilliseconds(100UL+mswaittime);�?�?�?�?�?�?
}
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
Configuring the ADC I am using the same values provided in the ADC Test Application (channel: 10).
The problem is after loading the program on the board, that the ADC sample values are not updating, but remaining on a constant value. Removing the jp12 jumper is setting the sample value to 1, but changing the resistor has no effect on the sample value.
Can you help me out what am I missing here?
Regards,
Marcell
#spc560p #adc #spc5studio #udetsk