SPC560P50L5 CAN Module doesn't work successfully
Hello everyone.
Because I need to test a newly purchased SPC560-DISP, I tested several commonly used modules
And these is my test devices:
Devices Used:
- MCU: SPC560P-DISP
- CAN: Kvaser Leaf LightV2
I conducted tests on several commonly used modules:
- PIT
- EIRQ
- PWM
- ADC
The test results for the above modules showed no issues. However, when testing the data transmission functionality of the CAN module:
- Loaded my own test program onto the development board.
- Kvaser and BUSMASTER were successfully connected.
Yet, I couldn't observe any data in BUSMASTER.
So, I replaced the SPC560P-DISP with another board of the same model that I had already and repeated the same steps in the same environment. Sadly, I could observe the values I intended to transmit in BUSMASTER.
What settings might I have overlooked that could cause this abnormal behavior? Or could the development board might be damaged?
Thanks
Louie