SPC582B SPI synchronous behaviour during ISR
Hi all,
I am using SPC582B mcu.
The system timer is based on PIT0 CH0 (default choice) at frequency 1kHz.
In the timer IRQ handler, I need to invoke SPI spi_lld_exchange API.
Problem is this API doesn't complete, remaining stuck on the while
SPC5_SPI_WAIT_FOR_TXRX_COMPLETION(spip);
SPI APIs are configured synchronous:

I already activated the preemptable ISR option in the configuration:

Since I don't know if the priority level is ascending or not, I tried both priority situations, that is:
System timer (PIT0 CH0) priority: 4 DSPI0 priority: 10
System timer (PIT0 CH0) priority: 10 DSPI0 priority:4
Is these some configuration flag or API to call in order to make this SPI API working?
Thank you all for any help or indication,
FP