Skip to main content
Explorer
April 19, 2024
Solved

SPC58ECxx C++ std::string throws linker errors

  • April 19, 2024
  • 1 reply
  • 1387 views

I'm working on a state machine for a console application, and I would like to use std::strings in C++, as they are much nicer to work with than C-style strings.

Including the string library does not result in errors, but when I call string objects in the code I start to get errors.  Here's an example of the code I am using:

//const char* output;		//No errors in c-style strings
std::string(output);		//Compiles, but results in linker error
switch(mState)
{
	case MAIN_STATE:
		output = "\r\nmain->";
		break;
	case CAN_STATE:
		output = "\r\ncan->";
		break;
	case UART_STATE:
		output = "\r\nuart->";
		break;
	case GPIO_STATE:
		output = "\r\ngpio->";
		break;
	default:
		output = "\r\nMAIN->";
		break;
}
//Print(output);	//No errors with C-style Strings
Print(output.c_str());	//Compiles, but results in linker error

 As I indicated in the code comments, any time I call a function from the <string> library, I get the following linker error:

07:41:57 **** Incremental Build of configuration Default for project ConsoleApp ****
make -j28 all 
Compiling cConsole.cpp
Linking build/out.elf
c:/spc5studio-6.0/eclipse/plugins/com.st.tools.spc5.tools.gnu.gcc.ppcvle.win32_4.9.4.20200908161514/toolchain/bin/../lib/gcc/powerpc-eabivle/4.9.4/../../../../powerpc-eabivle/lib/e200z4\libc.a(lib_a-abort.o): 
In function `abort':
abort.c:(.text.abort+0x10): undefined reference to `_exit'
c:/spc5studio-6.0/eclipse/plugins/com.st.tools.spc5.tools.gnu.gcc.ppcvle.win32_4.9.4.20200908161514/toolchain/bin/../lib/gcc/powerpc-eabivle/4.9.4/../../../../powerpc-eabivle/lib/e200z4\libc.a(lib_a-sbrkr.o): 
In function `_sbrk_r':
sbrkr.c:(.text._sbrk_r+0x1a): undefined reference to `sbrk'
c:/spc5studio-6.0/eclipse/plugins/com.st.tools.spc5.tools.gnu.gcc.ppcvle.win32_4.9.4.20200908161514/toolchain/bin/../lib/gcc/powerpc-eabivle/4.9.4/../../../../powerpc-eabivle/lib/e200z4\libc.a(lib_a-signalr.o): 
In function `_kill_r':
signalr.c:(.text._kill_r+0x1c): undefined reference to `kill'
c:/spc5studio-6.0/eclipse/plugins/com.st.tools.spc5.tools.gnu.gcc.ppcvle.win32_4.9.4.20200908161514/toolchain/bin/../lib/gcc/powerpc-eabivle/4.9.4/../../../../powerpc-eabivle/lib/e200z4\libc.a(lib_a-signalr.o): 
In function `_getpid_r':
signalr.c:(.text._getpid_r+0x0): undefined reference to `getpid'
collect2.exe: error: ld returned 1 exit status
make: *** [components/spc58ecxx_platform_component_rla/lib/rsc/rules.mk:164: build/out.elf] Error 1
"make -j28 all" terminated with exit code 2. Build might be incomplete.

07:42:06 Build Failed. 5 errors, 0 warnings. (took 9s.6ms)

 Interestingly, I've also noticed these kinds of errors with other standard C++ Libraries like <array> or <vector>.

These are my current linker settings:

Screenshot 2024-04-19 092256.png

 

 

 

 

 

 

 

 

What do I need to change in my linker settings to get the standard C++ libraries to link/build correctly?

This topic has been closed for replies.
Best answer by Erwan YVIN

Yes, it is possible but it is not so easy 

i recommend to follow to create the missing function in your project

Solved: SPC5Studio cannot use the malloc() and free() func... - STMicroelectronics Community

                 Best Regards

                                            Erwan

1 reply

Erwan YVIN
Erwan YVINBest answer
ST Employee
April 24, 2024

Yes, it is possible but it is not so easy 

i recommend to follow to create the missing function in your project

Solved: SPC5Studio cannot use the malloc() and free() func... - STMicroelectronics Community

                 Best Regards

                                            Erwan