SPC58xG : FCCU error CPU 0 lockstep disable
Hi
I try to apply the safety guide on the SPC58xG
The FCCU is a main part to check the error on the SPCx58, but I have several problems.
1) FCCU Status error.
The status register has this value (after clearing, and read flowing in x0A mode)
FCCU_RF_S0 = 0x00040000
FCCU_RF_S1 = 0x00000000
FCCU_RF_S2 = 0x00200000
FCCU_RF_S3 = 0x00078000
The FCCU_RF_S2 error corresponds to channel 85
In RM0391, table 17 , it Lockstep CPU0 Disable
When a Lauterbach is connected, this may be normal
But, when emulator is removed, there is the same error in my log file.
Why the CPU0 is not in lockstep mode ?
2) FCCU programmation
When a Lauterbach is connected, the FCCU change normally from NORMAL to CONFIG
The OPS bit, has state '1' pending , changes to '3' successful
But the same program, Lauterbach disconnect
The OPS bit, has state '1' pending , changes to '2' abort.
Why It's not possible to program FCCU ?
Regards