Associate
January 15, 2018
Solved
SPC5Studio build failure, too
- January 15, 2018
- 2 replies
- 3374 views
Posted on January 15, 2018 at 18:20
My problems same as
https://community.st.com/message/10560
The SPC5Studion was upgraded to 5.7.1
But I selected SPC56-DISCOVERY(BOARD) , DRIVERS --STM
My toolchains is the GNU make builder of spc5studio default.
Keep the example codes from code generation...
it is giving following errors,
- Symbol 'NULL' could not be resolved
- Symbol 'uint32_t' could not be resolved
- Symbol 'int32_t' could not be resolved
- Symbol 'uint16_t' could not be resolved
- Symbol 'uint8_t' could not be resolved
...
I was tried to set
in
C/C++ general ==> Preprocesseur Include
It cannot be to solved these problems.
Can you help me resolve these?
Thanks in advance for all your help.
Chamberplus
#spc56