SPC5Studio example application Error: Cannot load configuration file 'L/SPC56ELxx_RLA ADC Test Application for DiscoveryPlus/configuration.xml':
Hello (I am new to ST and SPC5Studio)
I just used the SPC5Studio Application Wizard to import the SPC56ELxx_RLA ADC Test Application for DiscoveryPlus and when I tried to generate it it showed the following error:
Error: Cannot load configuration file 'L/SPC56ELxx_RLA ADC Test Application for DiscoveryPlus/configuration.xml':
/SPC5-Config/application/instances/instance[7]/pit_settings/channel_0/frequency: Required Field.I tried repeating the process with the SPC56ELxx_RLA CAN Test Application for DiscoveryPlus with similar results. I can see a small 'x' in front of the configuration.xml file in the project explorer in both cases.
I really appreciate if someone could help me with this.
Thanks!
#cannot-load-configuration-file