SPC5Studio MarketplaceDiscoveryStrategy failed
Hello,
I have a very similar problem to that asked by
https://community.st.com/people/71687
on May 3, 2016. I have just installed SPC5Studio 5.7.1 and am attempting to use the Eclipse Marketplace to download the PowerPC-VLE GCC compiler as per the SPC5Studio installation instructions. When I click on Help->Eclipse Marketplace..., I (eventually) get a connection timeout:Connection to
failed on Connection timed out: connect.
I cannot access this URL via a browser. I cannot access
/external-link.jspa?url=http%3A%2F%2Fmarketplace.prod.spc5studio.com%2F
either. But I can access the software update onhttp://spc5.drive.cloudforge.com/projects/spc5releases/SPC5Studio/updates5
.Is there a current issue with the Marketplace? Alternatively, does anyone know what the URL is for the PowerPC-VLE GCC compiler so that I can point to it directly?
Thanks
Andrew
null