Skip to main content
Visitor II
March 8, 2024
Solved

UDE STK tool does not detect target client after new target configuration for SPC5746CBMKU6 board

  • March 8, 2024
  • 1 reply
  • 2617 views

I want to flash and debug using SPC5-UDESTK 5.02.04 on to the board SPC5746CBMKU6. This controller configuration is not given in the tool. So I have created new configuration for this board. Now I have tried to connect to target board. But it is failing to establish connection. 

shivani1_0-1709885305550.png

Connection and power supply is good(Tool LED glows). May be problem with target configuration. 

Attaching failed report and new target configuration file(in .txt, as .cfg is not supported here). Kindly provide the target configuration file for SPC5746CBMKU6, if you have. Or suggest edits in current file. 

 

This topic has been closed for replies.
Best answer by Erwan YVIN

Hello ,

The board SPC5746CBMKU6 is a processor coming from NXP side.

I recommend to check with them.

I do not known if there is PLS Ftdi in this board.

                   Best regards

                                Erwan

  

 

 

1 reply

Erwan YVIN
Erwan YVINBest answer
ST Employee
March 8, 2024

Hello ,

The board SPC5746CBMKU6 is a processor coming from NXP side.

I recommend to check with them.

I do not known if there is PLS Ftdi in this board.

                   Best regards

                                Erwan