Skip to main content
srosen
Associate
November 19, 2014
Question

Using CAN on SPC560B-DIS

  • November 19, 2014
  • 11 replies
  • 3280 views
Posted on November 19, 2014 at 16:24

Hello,

I am trying to make a simple project that for a start can send a single CAN frame.

I am using the SPC560B-DIS evb without any CAN board (will connect later on my own converter).

I took a CAN sample  from other evb and merged it to my project but it doesn't work!

Is there any CAN sample that works that I can use?

Can I connect a scope to the TX pin and view the data without converter to CAN High and CAN Low?

In the example i did not see any initialization to the I/O (Tx and Rx) is that correct?

Can I use the external clock on my board for the CAN module?

Thanks

Shachar
    This topic has been closed for replies.

    11 replies

    Erwan YVIN
    ST Employee
    October 15, 2015
    Posted on October 15, 2015 at 11:42

    Hello Sylvain ,

    i do not see any filters on your CAN configuration.

    How do you check your CAN Frame transmission ?

        Best Regards

                          Erwan