Skip to main content
Associate
August 4, 2025
Question

Adapt "How to build an AI app from scratch on STM32N6570-DK" to NUCLEO-N657X0-Q

  • August 4, 2025
  • 2 replies
  • 634 views

I am trying to make a minimal working example of a neural network running on the NUCLEO-N657X0-Q. To achieve this I followed this guide for the STM32N6570-DK on my own NUCLEO-N657X0-Q board. (https://community.st.com/t5/stm32-mcus/how-to-build-an-ai-application-from-scratch-on-the-stm32n6570-dk/ta-p/825591#!/825591)

However, CubeMX did not initialize the required code lines noted in the guide under "Important note 2".

Guide's screenshot:

sop_0-1754301835060.png

My screenshot:

sop_1-1754301835060.png

I did small address adaptions for the NUCLEO-N657X0-Q

  • LEDs: PG0, PG8
  • EXT_SMPS_MODE: PB12

I will attach the project below. Did I make a mistake or is CubeMX not able to configure the NUCLEO-N657X0-Q in the same way it supports the STM32N6570-DK yet? I also tried adding the lines from the screenshot of the guide myself, but it didn’t change the results and I assume there is more missing than is visible in the guide's screenshot.  I also assume the missing RIF and RIMC code lines are the main reason why the application didn’t work.

I still wrote all necessary files to flash, but the result is that I don’t get any messages from the serial port. Only the FSBL LED turns on and off again. The LED toggled in the Appli remains turned off.

I appreciate any help on this issue.

Is there another minimal AI example out for the Nucleo board, not the Discovery Kit?

Used SW:

CubeIDE 1.19.0

CubeMX 6.15.0

CubeProgrammer 2.20.0

X-Cube-AI 10.2.0

STM32Cube MCU package N6: 1.2.0

Used HW:

NUCLEO-N657X0-Q

OTP124=0x00008000

 

 

2 replies

Julian E.
Technical Moderator
August 4, 2025

Hello @sop,

 

I am doing the same thing to write an article on the Nucleo.

I am struggling with strange behaviors that I think come from CubeMX.

 

As you pointed out, sometimes it does not initialize the code for the RIF correctly, or the RAM.

 

I managed to create a project that works on the Nucleo, but I want to test it further before giving out the steps as I struggles to succeed 100% of the time. (I may do mistakes sometimes, but I feel like I have more issues when I use the standalone CubeMX than the one inside CubeIDE)

 

If I succeed replicating it, I should write the article quickly, as it is almost identical to the DK one.

 

Have a good day,
Julian

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
sopAuthor
Associate
August 22, 2025