Algobuilder GUI sensortilebox
Good morning everyone, I am trying to follow the example for machine learning given for the SensorTile Box
with Algobuilder.
I have followed all the steps with the configuration that did not give problems but when I go to compile the project it gives me this sequence of errors and I cannot flash the SensorTile Box.


Firmware Directory Initialization:
Firmware Directories Successfully Initialized!
Code generation finished successfully.
Build Process Started ...
Create.
Opening 'SensorTile.box-Project'.
11:51:40 **** Build of configuration SensorTile.box-Project for project SensorTile.box-Project ****
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Middlewares/ST/STM32_USB_Device_Library/Core/Src/usbd_core.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Middlewares/ST/STM32_USB_Device_Library/Core/Src/usbd_ctlreq.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Middlewares/ST/STM32_USB_Device_Library/Core/Src/usbd_ioreq.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Middlewares/ST/STM32_USB_Device_Library/Class/MSC/Src/usbd_msc.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Middlewares/ST/STM32_USB_Device_Library/Class/MSC/Src/usbd_msc_bot.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Middlewares/ST/STM32_USB_Device_Library/Class/MSC/Src/usbd_msc_data.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Middlewares/ST/STM32_USB_Device_Library/Class/MSC/Src/usbd_msc_scsi.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Middlewares/ST/STM32_USB_Device_Library/Class/CDC_MSC/Src/usbd_cdc_msc.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Middlewares/ST/STM32_USB_Device_Library/Class/CDC/Src/usbd_cdc.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Middlewares/Third_Party/FatFs/src/option/syscall.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Middlewares/Third_Party/FatFs/src/option/unicode.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Middlewares/Third_Party/FatFs/src/diskio.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Middlewares/Third_Party/FatFs/src/ff.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Middlewares/Third_Party/FatFs/src/ff_gen_drv.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Project/Src/algo_builder.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Project/Src/cube_hal_l4.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Project/Src/demo_serial.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Project/Src/fatfs.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Project/Src/main.c
Error: C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Project/Src/main.c: In function 'EnterDFU':
Error: C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Project/Src/main.c:1080:33: warning: array subscript 0 is outside array bounds of 'uint32_t[0]' {aka 'long unsigned int[]'} [-Warray-bounds]
Error: 1080 | JumpToDFU = (void (*)(void)) (*((uint32_t *)(0x00000000 + 4)));
Error: | ~^~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Project/Src/sd_diskio_SensorTile.box.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Project/Src/sensor_commands.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Project/Src/serial_protocol.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Project/Src/stm32l4xx_hal_msp.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Project/Src/stm32l4xx_it.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Project/Src/usbd_cdc_interface.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Project/Src/usbd_conf.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Project/Src/usbd_desc.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Project/Src/usbd_storage_if.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Project/Src/vcom.c
Example/SW4STM32/startup_stm32l4r9xx.o
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Project/CubeIDE/STM32L4R9ZI-SensorTile.box/syscalls.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Project/Src/ab_buffers.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Project/Src/ab_display.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Project/Src/ab_fft.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Project/Src/ab_sensor_hub.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Project/Src/ab_sequential_logic.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Project/Src/ab_signal.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Project/Src/ab_user_input.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Drivers/STM32L4xx_HAL_Driver/Src/stm32l4xx_hal.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Drivers/STM32L4xx_HAL_Driver/Src/stm32l4xx_hal_adc.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Drivers/STM32L4xx_HAL_Driver/Src/stm32l4xx_hal_adc_ex.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Drivers/STM32L4xx_HAL_Driver/Src/stm32l4xx_hal_cortex.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Drivers/STM32L4xx_HAL_Driver/Src/stm32l4xx_hal_dma.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Drivers/STM32L4xx_HAL_Driver/Src/stm32l4xx_hal_gpio.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Drivers/STM32L4xx_HAL_Driver/Src/stm32l4xx_hal_i2c.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Drivers/STM32L4xx_HAL_Driver/Src/stm32l4xx_hal_i2c_ex.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Drivers/STM32L4xx_HAL_Driver/Src/stm32l4xx_hal_pcd.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Drivers/STM32L4xx_HAL_Driver/Src/stm32l4xx_hal_pcd_ex.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Drivers/STM32L4xx_HAL_Driver/Src/stm32l4xx_hal_pwr.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Drivers/STM32L4xx_HAL_Driver/Src/stm32l4xx_hal_pwr_ex.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Drivers/STM32L4xx_HAL_Driver/Src/stm32l4xx_hal_rcc.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Drivers/STM32L4xx_HAL_Driver/Src/stm32l4xx_hal_rcc_ex.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Drivers/STM32L4xx_HAL_Driver/Src/stm32l4xx_hal_rtc.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Drivers/STM32L4xx_HAL_Driver/Src/stm32l4xx_hal_rtc_ex.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Drivers/STM32L4xx_HAL_Driver/Src/stm32l4xx_hal_sd.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Drivers/STM32L4xx_HAL_Driver/Src/stm32l4xx_hal_sd_ex.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Drivers/STM32L4xx_HAL_Driver/Src/stm32l4xx_hal_spi.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Drivers/STM32L4xx_HAL_Driver/Src/stm32l4xx_hal_tim.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Drivers/STM32L4xx_HAL_Driver/Src/stm32l4xx_hal_tim_ex.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Drivers/STM32L4xx_HAL_Driver/Src/stm32l4xx_ll_sdmmc.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Drivers/STM32L4xx_HAL_Driver/Src/stm32l4xx_ll_usb.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Project/Src/system_stm32l4xx.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Drivers/BSP/SensorTile.box/SensorTile.box.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Drivers/BSP/SensorTile.box/SensorTile.box_bus.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Drivers/BSP/SensorTile.box/SensorTile.box_env_sensors.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Drivers/BSP/SensorTile.box/SensorTile.box_env_sensors_ex.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Drivers/BSP/SensorTile.box/SensorTile.box_motion_sensors.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Drivers/BSP/SensorTile.box/SensorTile.box_motion_sensors_ex.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Drivers/BSP/SensorTile.box/SensorTile.box_sd.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Drivers/BSP/Components/hts221/hts221.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Drivers/BSP/Components/hts221/hts221_reg.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Drivers/BSP/Components/lis2mdl/lis2mdl.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Drivers/BSP/Components/lis2mdl/lis2mdl_reg.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Drivers/BSP/Components/lps22hh/lps22hh.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Drivers/BSP/Components/lps22hh/lps22hh_reg.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Drivers/BSP/Components/lsm6dsox/lsm6dsox.c
C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Drivers/BSP/Components/lsm6dsox/lsm6dsox_reg.c
Error: In function 'bytecpy',
Error: inlined from 'lsm6dsox_mode_set' at C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Drivers/BSP/Components/lsm6dsox/lsm6dsox_reg.c:13376:5:
Error: C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Drivers/BSP/Components/lsm6dsox/lsm6dsox_reg.c:96:13: warning: '*(uint8_t *)(&spi2_ctrl2_ois + offsetof(lsm6dsox_spi2_ctrl2_ois_t, hp_en_ois))' may be used uninitialized [-Wmaybe-uninitialized]
Error: 96 | *target = *source;
Error: | ~~~~~~~~^~~~~~~~~
Error: C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Drivers/BSP/Components/lsm6dsox/lsm6dsox_reg.c: In function 'lsm6dsox_mode_set':
Error: C:/Users/fr.silvano/STMicroelectronics/AlgoBuilder/FirmwareTemplate/Drivers/BSP/Components/lsm6dsox/lsm6dsox_reg.c:12866:29: note: '*(uint8_t *)(&spi2_ctrl2_ois + offsetof(lsm6dsox_spi2_ctrl2_ois_t, hp_en_ois))' was declared here
Error: 12866 | lsm6dsox_spi2_ctrl2_ois_t spi2_ctrl2_ois;
Error: | ^~~~~~~~~~~~~~
SensorTile.box-Project.elf
Error: C:/ST/STM32CubeIDE_1.15.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.12.3.rel1.win32_1.0.100.202403111256/tools/bin/../lib/gcc/arm-none-eabi/12.3.1/../../../../arm-none-eabi/bin/ld.exe: warning: SensorTile.box-Project.elf has a LOAD segment with RWX permissions
arm-none-eabi-size SensorTile.box-Project.elf
text data bss dec hex filename
105648 2920 45048 153616 25810 SensorTile.box-Project.elf
11:54:15 Build Finished. 0 errors, 3 warnings. (took 2m:35s.373ms)
Build Process Finished
Exit Code: 0

What can I do to resolve this issue?