Cube AI studio: build fails after editing .ioc file.
Whenever I am starting to make project from scratch in STM32Cube AI studio, It gives complete structure with .ioc files as well as AI files, but as soon as I make changes in .ioc file and generate code after loading in CubeIDE, it changes the middlewares and build error comes . What is the solution for that?
1. Should I first make the .ioc project and then make project in STM32Cube AI studio ( Import the existing project from STM32CubeMX or STM32Cube AI studio)
2. Another doubt is if I make project from preexisting .ioc, Do I need project in application mode for that as AI changes will work in application mode only ( but STM32N6 doesnt work without FSBL), what is your suggestion for Edge AI project building?
The error was :
Description Resource Path Location Type make: *** No rule to make target 'C:/Users/hp/.stm32cubeaistudio/workspace/Modified_STM32/Middlewares/ST/AI/Npu/ecloader.c', needed by 'Middlewares/ST/AI/Npu/ecloader.o'. Stop. Modified_STM32_Appli C/C++ Problem
Thanks & Regards
Chanchal