Skip to main content
Associate II
November 29, 2025
Solved

Data Format Output by YOLOv8n_float Model Running on Cube.AI via STM32N6570-DK

  • November 29, 2025
  • 1 reply
  • 245 views

Dear ST staff, Recently, while using STM32CubeMX with CubeAI to deploy the yolov8n_192_quant_pc_uf_od_coco-person.tflite model from object_detection onto the STM32N6570-DK development board.

_0-1764443989806.png

        Subsequently, following CubeAI's configuration, I programmed the network_atonbuf.xSPI2.bin file into the 0x71000000 memory location

_1-1764444130600.png

It is worth noting that this model is of type float, not int8 quantisation (as I understand it), and both member pointers in

LL_Buffer_InfoTypeDef's

const float *scale; /**< */

const int16_t *offset;


are NULL. This should indicate that the output requires no normalisation conversion.

void MX_X_CUBE_AI_Process(void)
{
 /* USER CODE BEGIN 6 */
 LL_ATON_RT_RetValues_t ll_aton_rt_ret = LL_ATON_RT_DONE;
 const LL_Buffer_InfoTypeDef * ibuffersInfos = NN_Interface_Default.input_buffers_info();
 const LL_Buffer_InfoTypeDef * obuffersInfos = NN_Interface_Default.output_buffers_info();
 buffer_in = (uint8_t *)LL_Buffer_addr_start(&ibuffersInfos[0]);
 buffer_out = (uint8_t *)LL_Buffer_addr_start(&obuffersInfos[0]);
 printf("buffer_in addr=%p\n", buffer_in);
 printf("buffer_in addr mod4=%ld\n", ((uintptr_t)buffer_in)%4);
 printf("buffer_in addr mod8=%ld\n", ((uintptr_t)buffer_in)%8);
 HAL_LTDC_SetAddress(&hltdc, buffer_in, 1);
 HAL_DCMIPP_CSI_PIPE_Start(&hdcmipp, DCMIPP_PIPE2, DCMIPP_VIRTUAL_CHANNEL0 , buffer_in, DCMIPP_MODE_SNAPSHOT);
 HAL_Delay(5);
 LL_ATON_RT_RuntimeInit();

 // run 1 inferences
 for (int inferenceNb = 0; inferenceNb<1; ++inferenceNb) {
 /* ------------- */
 /* - Inference - */
 /* ------------- */
 /* Pre-process and fill the input buffer */
 //_pre_process(buffer_in);

 /* Perform the inference */
 LL_ATON_RT_Init_Network(&NN_Instance_Default);
 do {
 ll_aton_rt_ret = LL_ATON_RT_RunEpochBlock(&NN_Instance_Default);
 if (ll_aton_rt_ret == LL_ATON_RT_WFE) {
 LL_ATON_OSAL_WFE();
 }
 } while (ll_aton_rt_ret != LL_ATON_RT_DONE);

 /* Post-process the output buffer */

 /* ------------------ 替换这里的 Post-process 区块 ------------------ */
 {
			#define CONF_THRESHOLD 0.3f // 根据模型调试设定

 	int channels = (int)obuffersInfos->mem_shape[1]; // 5
 	int num_boxes = (int)obuffersInfos->mem_shape[2]; // 756
 	int total_elems = channels * num_boxes;

 	uint8_t *tmp = (uint8_t *)buffer_out;
 	int nn_out_len_bytes = channels * num_boxes * sizeof(float);
 	SCB_InvalidateDCache_by_Addr((uint32_t *)tmp, nn_out_len_bytes);
 	for(int i = 0;i<756;i++)
 	{
 		printf("A:%.2f\r\n",((float*)buffer_out)[i+4*num_boxes]);
 	}

 }



 LL_ATON_RT_DeInit_Network(&NN_Instance_Default);
 /* -------------------- */
 /* - End of Inference - */
 /* -------------------- */
 }
 LL_ATON_RT_RuntimeDeInit();
 /* USER CODE END 6 */
}

    I have attempted numerous methods to parse YOLOv8n data, but frequently encounter anomalous values, particularly when seeking configuration details within the [1x5x756] structure, where many values are disproportionately large.

_2-1764444392236.png

Is there any relevant ST analysis data documentation available for reference?

 

Best answer by Julian E.

Hi @实在太懒于是不想取名,

 

First of all, the model is quantized in int8, it is just that the input and output are float32 (converted to or from).

 

Then in your case, I think you should compare the C model output and the original tflite output.

To do so, in a first step, you should use the "validation on target" from X Cube AI or do it manually: 

https://stedgeai-dc.st.com/documentation 

 

You want to look at the COS, if close to 1 then at least your output the one expected.

 

Then, maybe you don't print them correctly. To know that I suggest you use the AI Runner to get the output of the C model and compare them to the tflite model

 

Documentation: https://stedgeai-dc.st.com/assets/embedded-docs/ai_runner_python_module.html

 

The AI runner can be found here: \ST\STEdgeAI\2.2\scripts\ai_runner

  • First, you need to install the requirements: pip install -r requierement.txt.
  • Then you need to load the validation firmware with the n6_loader.py (which assumes you did the generate)
  • Open a git bash (in ai_runner folder) and run:
    export PROTOCOL_BUFFERS_PYTHON_IMPLEMENTATION=python
  • Then run: python ./example/checker.py -d serial:921600

 

By default, the AI checker do…

But you can edit it to:

  • Load your dataset (npz)
  • Save up the outputs

To do so, open checker.py

JulianE_0-1764860262446.png

 

  • Comment the line 62 and replace it to load your dataset:
    inputs = np.load(“./dataset.npy)
  • Save ‘outputs’ after the line 64 with something like: np.save("./ output.npy", outputs)
  • Comment line 66

Run again the checker.py and you should get the output saved.

 

Finally, in another python script or notebook, you can:

  • Load your dataset
  • Use the onnx runtime to get your original model outputs (or load them if you already have them
  • Load the N6 output
  • Run any tests you would like

 

Have a good day,

Julian

1 reply

Julian E.
Julian E.Best answer
Technical Moderator
December 4, 2025

Hi @实在太懒于是不想取名,

 

First of all, the model is quantized in int8, it is just that the input and output are float32 (converted to or from).

 

Then in your case, I think you should compare the C model output and the original tflite output.

To do so, in a first step, you should use the "validation on target" from X Cube AI or do it manually: 

https://stedgeai-dc.st.com/documentation 

 

You want to look at the COS, if close to 1 then at least your output the one expected.

 

Then, maybe you don't print them correctly. To know that I suggest you use the AI Runner to get the output of the C model and compare them to the tflite model

 

Documentation: https://stedgeai-dc.st.com/assets/embedded-docs/ai_runner_python_module.html

 

The AI runner can be found here: \ST\STEdgeAI\2.2\scripts\ai_runner

  • First, you need to install the requirements: pip install -r requierement.txt.
  • Then you need to load the validation firmware with the n6_loader.py (which assumes you did the generate)
  • Open a git bash (in ai_runner folder) and run:
    export PROTOCOL_BUFFERS_PYTHON_IMPLEMENTATION=python
  • Then run: python ./example/checker.py -d serial:921600

 

By default, the AI checker do…

But you can edit it to:

  • Load your dataset (npz)
  • Save up the outputs

To do so, open checker.py

JulianE_0-1764860262446.png

 

  • Comment the line 62 and replace it to load your dataset:
    inputs = np.load(“./dataset.npy)
  • Save ‘outputs’ after the line 64 with something like: np.save("./ output.npy", outputs)
  • Comment line 66

Run again the checker.py and you should get the output saved.

 

Finally, in another python script or notebook, you can:

  • Load your dataset
  • Use the onnx runtime to get your original model outputs (or load them if you already have them
  • Load the N6 output
  • Run any tests you would like

 

Have a good day,

Julian

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Associate II
December 5, 2025

Thank you for your reply. I believe I have identified the root cause of the issue: I had not configured the NPU option in RIF. After enabling it, all outputs now fall between 0 and 1.