Skip to main content
Associate III
May 22, 2025
Question

Help, stm32N6 fails to use st-mnist, no response.

  • May 22, 2025
  • 1 reply
  • 364 views

Please help, why can my configuration of flower work normally, but when I change the model st-minst and follow the same steps to deploy and burn, the LCD screen does not light up and the model does not work.

e5a0cfc93a70cd839e50062ca44e1d0.jpg

42ab770809de4deb1b4cb8934b082ce.jpg

1 reply

LQC_Author
Associate III
May 22, 2025

Hello, I use st-minst in ST Model Zoo to deploy my project, but when I burned stm32N6570_DK, it didn't work. However, I tried flower and food and they both worked fine. Why can't st-minst work? Are there other steps required?
This is my command and .yaml content

python stm32ai_main.py --config-path ./src/config_file_examples/ --config-name deployment_n6_config.yaml
general:
 # path to a `.tflite` or `.onnx` file.
# model_path: ../../stm32ai-modelzoo/image_classification/mobilenetv2/ST_pretrainedmodel_public_dataset/flowers/mobilenet_v2_0.35_128_fft/mobilenet_v2_0.35_128_fft_int8.tflite
 model_path: ../../stm32ai-modelzoo/image_classification/st_mnist/ST_pretrainedmodel_public_dataset/emnist_byclass/st_mnist_v1_28_tfs/st_mnist_v1_28_tfs_int8.tflite
# model_path: ../../stm32ai-modelzoo/image_classification/mobilenetv2/ST_pretrainedmodel_public_dataset\food-101\mobilenet_v2_0.35_128_fft/mobilenet_v2_0.35_128_fft_int8.tflite
operation_mode: deployment

dataset:
# name: flowers_dataset
# class_names: [daisy, dandelion, roses, sunflowers, tulips]
 name: hande
 class_names: [A,B,C,D,E,F,G,H,I,J,K,L,M,N,O,P,Q,R,S,T,U,V,W,X,Y,Z]
# name: food-101
# class_names: [apple_pie,baby_back_ribs,baklava,beef_carpaccio,beef_tartare,beet_salad,beignets,bibimbap,bread_pudding,breakfast_burrito,bruschetta,caesarsalad,cannoli,caprese_salad,carrot_cake,ceviche,cheesecake,cheese_plate,chicken_curry,chicken_quesadilla,chicken_wings,chocolate_cake,chocolte_mousse,churros,clam_chowder,club_sandwich,crab_cakes,creme_brulee,croque_madame,cup_cakes,deviled_eggs,donuts,dumplings,edamame,eggs_beneict,escargots,falafel,filet_mignon,fish_and_chips,foie_gras,french_fries,french_onion_soup,french_toast,fried_calamari,fried_rice,frozen_yogrt,garlic_bread,gnocchi,greek_salad,grilled_cheese_sandwich,grilled_salmon,guacamole,gyoza,hamburger,hot_and_sour_soup,hot_dog,huevos_rancheos,hummus,ice_cream,lasagna,lobster_bisque,lobster_roll_sandwich,macaroni_and_cheese,macarons,miso_soup,mussels,nachos,omelette,onion_rings,oysters,pad_hai,paella,pancakes,panna_cotta,peking_duck,pho,pizza,pork_chop,poutine,prime_rib,pulled_pork_sandwich,ramen,ravioli,red_velvet_cake,risotto,smosa,sashimi,scallops,seaweed_salad,shrimp_and_grits,spaghetti_bolognese,spaghetti_carbonara,spring_rolls,steak,strawberry_shortcake,sushi,tacs,takoyaki,tiramisu,tuna_tartare,waffles]
preprocessing:
 resizing:
 interpolation: bilinear
 aspect_ratio: crop
 color_mode: rgb # rgb, bgr

tools:
 stedgeai:
 version: 10.1.0
 optimization: balanced
 on_cloud: False # Not Available For STM32N6
 path_to_stedgeai: D:/16_STEdgeAI/2.1/Utilities/windows/stedgeai.exe
 path_to_cubeIDE: D:/15_STM32CubeIDE_1.18.0/stm32cubeide1.17/STM32CubeIDE_1.17.0/STM32CubeIDE/stm32cubeide.exe

deployment:
 c_project_path: ../application_code/image_classification/STM32N6/
 IDE: GCC
 verbosity: 1
 hardware_setup:
 serie: STM32N6
 board: STM32N6570-DK

hydra:
 run:
 dir: ./src/experiments_outputs/${now:%Y_%m_%d_%H_%M_%S}

mlflow:
 uri: ./src/experiments_outputs/mlruns

 

Julian E.
Technical Moderator
May 23, 2025

Hello @LQC_ ,

 

The Mnist model was trained using grayscale images but the deployment on N6 does not support mnist so I would not advise you to use it.

 

That being said, I could not reproduce your issue.

  • Are you using a usb C to usb C cable? In some case, you can have issues because of the power supply.
  • Did you unplug/plug again the board after switching the pins to the left?
  • Do you get any errors during the deployment?

 

You cubeIDE path is very strange, maybe it comes from that.

You may try to create a new clean install of model zoo.

 

I attached my exact yaml for reference.

 

Have a good day,

Julian

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.