Hi, i have recorded some data using the BLE option with STWINKt1b. the file are .dat file, how do i convert it to CSV or better how do i import the files to Unico in order to build a configuration for the ISM330DHCX ? thanks in advance :)
..
..
Hi @TS.2 ,
you might use the High Speed Datalog function pack, as reported in the user manual UM2688 (p. 31), you can use an already available python script (folder \Utilities\Python_SDK\).
In particular, the hsdatalog_to_unico.py can prepare data to be imported into Unico-GUI. You can find it in the, but I attach it to this post for completeness.
As second step, you might need to charge again the .ucf file on the STWIN, in order to configure the ISM330DHCX.
For this scope, you can check the procedure I've reported here below:
Run the example with STWIN and HSDatalog
HSDatalog is a high speed data logging command line application for the STWIN board.
HSDatalog also allows configuring ISM330DHCX Machine learning Core and reading the output of the selected algorithm.
Here all the required steps to run a MLC example through STWIN and HSDatalog:
If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster.
-Eleon
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.