how can i print the values via n-Class Classification library
Hello,
I am a beginner
I downloaded the STM32-NANOEDGE-DATALOGGER firmware via the github link.
This STM32-NANOEDGE-DATALOGGER is used in NaoedgeAIStudio and is streaming data via UART (VCOM port) from STLink.
but I see that the example is only given for an AD (Anomaly Detection) project and I'd like to know how to modify it for an n-Class project?
Also, is it possible to add the USB_CDC_ACM class to activate the VCOM port on the STWIN.box without the STLink?
If so, how do I do it?
Board used: STWIN.box