Skip to main content
Evelina CAMILLERI
ST Employee
November 11, 2022
Question

Is the ISM330ISN the only product with the ISPU? If yes, all those can be programmed with the NEAI studio?

  • November 11, 2022
  • 1 reply
  • 816 views

..

This topic has been closed for replies.

1 reply

Luca SEGHIZZI
Senior
November 11, 2022

There are more products using the ISPU on top of the one used for the webinar, however, the ISM330ISN is the only one which can be programmed using the NEAI studio SW tool. The other products are the ISM330IS which is the industrial version of an ISPU device that doesn't have the possibility to program with the NEAI, but only with C language and we have the same for the LSM6DSO16IS which is the consumer part number, these two part numbers can be used easily with the X-CUBE-ISPU software package.