Issue with --input-data-type --inputs-ch-position --output-data-type in ST Edge AI 2.1.0
Hello everyone,
I encountered an issue while using ST Edge AI 2.1.0 and I would appreciate some help.
Here is my original CUSTOM_MPOOLS configuration, which worked perfectly:
However, when I added the following options to the options section:
I received the following error:
I referred to the official documentation and saw that it does mention using these commands to modify the input/output requirements of the model. However, it seems that these commands are not fully supported in ST Edge AI 2.1.0, which is causing the error above.

My questions are:
Why does adding --input-data-type uint8 --inputs-ch-position chlast --output-data-type float32 cause this error?
Are these commands incompatible with ST Edge AI 2.1.0, or is there another configuration issue?
Is there another way to modify the input/output data formats, or are there specific things I need to be aware of?
Thank you in advance for your help!