LL_ATON_RT_Reset_Network() call between inferences
Hi,
On my test setup with the NN (MiniResNet model from STM32 Model Zoo),
I observed the following behavior:
Without calling LL_ATON_RT_Reset_Network() after each inference, only the first inference runs a few ms. All subsequent calls return almost instantly (execution time ≈ 0), and no inference is actually performed.
With LL_ATON_RT_Reset_Network() invoked either before or after each inference (as in the example below), every inference is executed normally.
Questions:
1. Is calling LL_ATON_RT_Reset_Network() always required to ensure correct inference execution? Are there any cases where the LL_ATON_RT_Reset_Network() call is not needed?
2. In the case of stateful neural networks (e.g. RNN), is it safe to call LL_ATON_RT_Reset_Network()? Will the network’s state remain intact, or is it cleared/reset as well?
while(1){
/* ------------- */
/* - Inference - */
/* ------------- */
/* Pre-process and fill the input buffer */
//_pre_process(buffer_in);
/* Perform the inference */
LL_ATON_RT_Reset_Network(&NN_Instance_Default);
printf("Starting inference");
do {
/* Execute first/next step */
ll_aton_rt_ret = LL_ATON_RT_RunEpochBlock(&NN_Instance_Default);
/* Wait for next event */
if (ll_aton_rt_ret == LL_ATON_RT_WFE)
LL_ATON_OSAL_WFE();
} while (ll_aton_rt_ret != LL_ATON_RT_DONE);
/* Post-process the output buffer */
/* Invalidate the associated CPU cache region if requested */
//_post_process(buffer_out);
/* -------------------- */
/* - End of Inference - */
/* -------------------- */
}