NanoEdge AI : not data is flowing when loading data from serial (USB)
Hi,
I am running a project on NanoEdge AI (anomaly detection), using STEVAL-STWINKT1B SensorTile Wireless Industrial Node and STLINK-V3MINI. I am following st's youtube turotial NanoEdge AI Studio V3 - Anomaly Detection demo. I would like to load data from serial (USB), but no data is flowing.
What I did so far (mosty what is said in um2622) :
- Connected USB to the board while keeping USR button pressed
- Connected STLINK-V3MINI
- Erased all sectors and loaded DataLogExtended.bin into the board ( path fp-sns-stbox1\STM32CubeFunctionPack_FP-SNS-STBOX1_V1.6.0\Projects\STM32L4R9ZI-SensorTile.box\Applications\DataLogExtended\Binary)
- Loaded DataLogExtended.bin into STWIN-v3MINI ( path fp-sns-stbox1\STM32CubeFunctionPack_FP-SNS-STBOX1_V1.6.0\Projects\STM32L4R9ZI-SensorTile.box\Applications\DataLogExtended\Binary )
- Disconnected the board and STLINK-V3MINI and long pressed RESET button
- Reconnected the board first, and then STLINK-V3MINI
- at this step COM3 and COM4 both appear in device manager:

- Opened Nanoedge AI Studio
- Tried to import signals (regular ones) from USB using both COM port (COM 3) and COM4 (the virtual one) but when clicking "Start/STOP", data don't show up (see the following image) :

I have checked UART configuration and baud rate, parity, data bits, stop bits seem correct :

I also installed Tera Term to check if data is collected from COM3 and COM4 when clicking "Start/STOP"... it seems nothing is out.

There are probably steps I am missing but it is not clear to me how it works. Can I know the steps I should follow ?
Best,
Anthony