NanoEdgeAIStudio : is it possible to log ultrasounds ? (STWINKT1B)
Hi,
I am using NanoEdgeAIStudio to detect anomalies on microphone signal. I am particularly interested in logging ultrasounds (from 20kHz to 100kHz).
I used the Datalogger tool (in NanoEdgeAIStudio) to set up the datalogger and generate the neai_datalog.bin file. In this tool, I have noticed the only microphone available is "MP23ABS1" (see the screenshot below). I have read MP23ABS1's doc, though it is not clear to me if it is able to log ultrasounds ? Can you clarify this pls ?

Also, I have read STWINKT1B's doc and I know there is also microphone IMP23ABSU (for ultrasounds, with a bandwidth up to 80kHz, as indicated in the doc). I would prefer to use IMP23ABSU instead of MP23ABS1 to log the data in NanoEdgeAIStudio. Is that possible ?
To clarify, I would like to collect data from microphone IMP23ABSU (using the tool "import signal" and "from serial (USB)", as below). So far, I set up a project using sensor type "Microphone sensor 1 axis", ODR=100000Hz, sample size=4096, and I succeeded in logging microphone data... data show up in "serial output", but I am not sure which microphone the data come from. Do you have any idea ?

Thanks
Anthony