Skip to main content
Visitor II
October 22, 2025
Question

Need Help to run Yolov8n inference on NUCLEO-U575ZI-Q

  • October 22, 2025
  • 1 reply
  • 146 views

Hey I am very new to this world. I study Data science and AI and I am currently writing my thesis on Federated Learning on Edge Devices.

I am currently really really struggling on the device side. I have a quantized Yolov8n model fine tuned on weed detection dataset. My goal is to first upload the model onto my board which is a NUCLEO-U575ZI-Q with STM32U575ZIT6QU mcu. I tried the systemPerformance template from X-Cube-AI it works but I can not manage to run my code (mostly ChatGPTs). I tried a lot of different things but could only make the device print over UART for now. I need someone who is familiar with the app and mcu programming. Here is the code of my last attempt which failed. I tried to follow DigiKey's X-Cube-AI tutorial. The device seems to crash into the void HardFault_Handler(void).

Here is my main.c :

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2025 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "app_x-cube-ai.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include <stdio.h>

#include "ai_datatypes_defines.h"
#include "ai_platform.h"
#include "yolov8n.h"
#include "yolov8n_data.h"
/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/

CRC_HandleTypeDef hcrc;

TIM_HandleTypeDef htim16;

UART_HandleTypeDef huart1;

/* USER CODE BEGIN PV */
uint8_t msg[] = "Hello from USART3\r\n";
/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void SystemPower_Config(void);
static void MX_GPIO_Init(void);
static void MX_ICACHE_Init(void);
static void MX_CRC_Init(void);
static void MX_TIM16_Init(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */

/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{
 /* USER CODE BEGIN 1 */
	char buf[50];
	int buf_len = 0;
	ai_error ai_err;
	ai_i32 nbatch;
	uint32_t timestamp;
	float y_val;

	// Chunk of memory used to hold intermediate values for neural network
	AI_ALIGNED(4) ai_u8 activations[AI_YOLOV8N_DATA_ACTIVATIONS_SIZE];

	// Buffers used to store input and output tensors
	AI_ALIGNED(4) ai_i8 in_data[AI_YOLOV8N_IN_1_SIZE_BYTES];
	AI_ALIGNED(4) ai_i8 out_data[AI_YOLOV8N_OUT_1_SIZE_BYTES];

	// Pointer to our model
	ai_handle yolov8n = AI_HANDLE_NULL;

	// Initialize wrapper structs that hold pointers to data and info about the
	// data (tensor height, width, channels)
	// Input/Output buffer handles
	ai_buffer *ai_input;
	ai_buffer *ai_output;

	// Get I/O buffer descriptors at runtime
	ai_input = ai_yolov8n_inputs_get(AI_HANDLE_NULL, NULL);
	ai_output = ai_yolov8n_outputs_get(AI_HANDLE_NULL, NULL);

	// Fill network parameters at runtime
	ai_network_params ai_params;
	ai_params.params = ai_yolov8n_data_weights_buffer_get(ai_yolov8n_data_weights_get());
	ai_params.activations = ai_yolov8n_data_activations_buffer_get(activations);


	// Set pointers wrapper structs to our data buffers
	ai_input[0].data = AI_HANDLE_PTR(in_data);
	ai_output[0].data = AI_HANDLE_PTR(out_data);
 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */
 /* USER CODE END Init */

 /* Configure the System Power */
 SystemPower_Config();

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_ICACHE_Init();
 MX_CRC_Init();
 MX_TIM16_Init();
 MX_X_CUBE_AI_Init();
 /* USER CODE BEGIN 2 */
 	HAL_UART_Transmit(&huart1, msg, sizeof(msg), 100);
	// Start timer/counter
	HAL_TIM_Base_Start(&htim16);

	// Greetings!
	buf_len = sprintf(buf, "\r\n\r\nSTM32 X-Cube-AI test\r\n");
	HAL_UART_Transmit(&huart1, (uint8_t *)buf, buf_len, 100);

	// Create instance of neural network
	ai_err = ai_yolov8n_create(&yolov8n, AI_YOLOV8N_DATA_CONFIG);
	if (ai_err.type != AI_ERROR_NONE)
	{
	 buf_len = sprintf(buf, "Error: could not create NN instance\r\n");
	 HAL_UART_Transmit(&huart1, (uint8_t *)buf, buf_len, 100);
	 while(1);
	}

	// Initialize neural network
	if (!ai_yolov8n_init(yolov8n, &ai_params))
	{
	 buf_len = sprintf(buf, "Error: could not initialize NN\r\n");
	 HAL_UART_Transmit(&huart1, (uint8_t *)buf, buf_len, 100);
	 while(1);
	}
 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
	// Fill input buffer (use test value)
	for (uint32_t i = 0; i < AI_YOLOV8N_IN_1_SIZE; i++)
	{
	((ai_float *)in_data)[i] = (ai_float)2.0f;
	}

	// Get current timestamp
	timestamp = htim16.Instance->CNT;

	// Perform inference
	nbatch = ai_yolov8n_run(yolov8n, &ai_input[0], &ai_output[0]);
	if (nbatch != 1) {
	buf_len = sprintf(buf, "Error: could not run inference\r\n");
	HAL_UART_Transmit(&huart1, (uint8_t *)buf, buf_len, 100);
	}

	// Read output (predicted y) of neural network
	y_val = ((float *)out_data)[0];

	// Print output of neural network along with inference time (microseconds)
	buf_len = sprintf(buf,
					"Output: %f | Duration: %lu\r\n",
					y_val,
					htim16.Instance->CNT - timestamp);
	HAL_UART_Transmit(&huart1, (uint8_t *)buf, buf_len, 100);

	// Wait before doing it again
	HAL_Delay(500);
 /* USER CODE END WHILE */

 //MX_X_CUBE_AI_Process();
 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Configure the main internal regulator output voltage
 */
 if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
 RCC_OscInitStruct.PLL.PLLMBOOST = RCC_PLLMBOOST_DIV1;
 RCC_OscInitStruct.PLL.PLLM = 1;
 RCC_OscInitStruct.PLL.PLLN = 10;
 RCC_OscInitStruct.PLL.PLLP = 2;
 RCC_OscInitStruct.PLL.PLLQ = 2;
 RCC_OscInitStruct.PLL.PLLR = 1;
 RCC_OscInitStruct.PLL.PLLRGE = RCC_PLLVCIRANGE_1;
 RCC_OscInitStruct.PLL.PLLFRACN = 0;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
 |RCC_CLOCKTYPE_PCLK3;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB3CLKDivider = RCC_HCLK_DIV1;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4) != HAL_OK)
 {
 Error_Handler();
 }
}

/**
 * @brief Power Configuration
 * @retval None
 */
static void SystemPower_Config(void)
{

 /*
 * Switch to SMPS regulator instead of LDO
 */
 if (HAL_PWREx_ConfigSupply(PWR_SMPS_SUPPLY) != HAL_OK)
 {
 Error_Handler();
 }
/* USER CODE BEGIN PWR */
/* USER CODE END PWR */
}

/**
 * @brief CRC Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_CRC_Init(void)
{

 /* USER CODE BEGIN CRC_Init 0 */

 /* USER CODE END CRC_Init 0 */

 /* USER CODE BEGIN CRC_Init 1 */

 /* USER CODE END CRC_Init 1 */
 hcrc.Instance = CRC;
 hcrc.Init.DefaultPolynomialUse = DEFAULT_POLYNOMIAL_ENABLE;
 hcrc.Init.DefaultInitValueUse = DEFAULT_INIT_VALUE_ENABLE;
 hcrc.Init.InputDataInversionMode = CRC_INPUTDATA_INVERSION_NONE;
 hcrc.Init.OutputDataInversionMode = CRC_OUTPUTDATA_INVERSION_DISABLE;
 hcrc.InputDataFormat = CRC_INPUTDATA_FORMAT_BYTES;
 if (HAL_CRC_Init(&hcrc) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN CRC_Init 2 */

 /* USER CODE END CRC_Init 2 */

}

/**
 * @brief ICACHE Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_ICACHE_Init(void)
{

 /* USER CODE BEGIN ICACHE_Init 0 */

 /* USER CODE END ICACHE_Init 0 */

 /* USER CODE BEGIN ICACHE_Init 1 */

 /* USER CODE END ICACHE_Init 1 */

 /** Enable instruction cache (default 2-ways set associative cache)
 */
 if (HAL_ICACHE_Enable() != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ICACHE_Init 2 */

 /* USER CODE END ICACHE_Init 2 */

}

/**
 * @brief TIM16 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_TIM16_Init(void)
{

 /* USER CODE BEGIN TIM16_Init 0 */

 /* USER CODE END TIM16_Init 0 */

 /* USER CODE BEGIN TIM16_Init 1 */

 /* USER CODE END TIM16_Init 1 */
 htim16.Instance = TIM16;
 htim16.Init.Prescaler = 80 - 1;
 htim16.Init.CounterMode = TIM_COUNTERMODE_UP;
 htim16.Init.Period = 65535;
 htim16.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
 htim16.Init.RepetitionCounter = 0;
 htim16.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
 if (HAL_TIM_Base_Init(&htim16) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN TIM16_Init 2 */

 /* USER CODE END TIM16_Init 2 */

}

/**
 * @brief USART1 Initialization Function
 * @PAram None
 * @retval None
 */
void MX_USART1_UART_Init(void)
{

 /* USER CODE BEGIN USART1_Init 0 */

 /* USER CODE END USART1_Init 0 */

 /* USER CODE BEGIN USART1_Init 1 */

 /* USER CODE END USART1_Init 1 */
 huart1.Instance = USART1;
 huart1.Init.BaudRate = 1000000;
 huart1.Init.WordLength = UART_WORDLENGTH_8B;
 huart1.Init.StopBits = UART_STOPBITS_1;
 huart1.Init.Parity = UART_PARITY_NONE;
 huart1.Init.Mode = UART_MODE_TX_RX;
 huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
 huart1.Init.OverSampling = UART_OVERSAMPLING_16;
 huart1.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
 huart1.Init.ClockPrescaler = UART_PRESCALER_DIV1;
 huart1.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
 if (HAL_UART_Init(&huart1) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_SetTxFifoThreshold(&huart1, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_SetRxFifoThreshold(&huart1, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_DisableFifoMode(&huart1) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN USART1_Init 2 */

 /* USER CODE END USART1_Init 2 */

}

/**
 * @brief GPIO Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 /* USER CODE BEGIN MX_GPIO_Init_1 */

 /* USER CODE END MX_GPIO_Init_1 */

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOA_CLK_ENABLE();

 /* USER CODE BEGIN MX_GPIO_Init_2 */

 /* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */

/* USER CODE END 4 */

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @PAram file: pointer to the source file name
 * @PAram line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

 

I would really appreciate any help. I will also have to calculate backpropagation for the federated learning so anyone who's nice enough to mentor me for this project is welcomed.

Thank you,

Adhygame

1 reply

Julian E.
Technical Moderator
October 29, 2025

Hi @Adhygame,

 

This tutorial may help you.

Be careful to use cubeMX standalone and the N6 cube package 1.1.1.

The N6 is pretty badly supported on the cubeMX...

 

How to build an AI application from scratch on the... - STMicroelectronics Community

 

Note that the N6 is most likely the most complex STM32 to use.

 

I don't know what your goal is, but you may be able to do some things without the need to create an embedded application:

  1. You have the dev cloud to easily benchmark the model inference time on N6: Home - ST Edge AI Developer Cloud
  2. You also have the validation script to help you compare results between the embedded model and onnx model:Getting started - How to evaluate a model on STM32N6 board
  3. You also have the AI runner: How to use the AiRunner package

 

Have a good day,

Julian

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.