Skip to main content
Associate II
April 20, 2025
Question

Need Help with FCNN Model: Unable to Get Output from Input Data

  • April 20, 2025
  • 1 reply
  • 535 views

Hello STM Community,

I have a question regarding my FCNN model. My goal is to feed input data into the model and obtain the corresponding output, but I haven’t been successful so far. Could you please assist me with this? Any guidance would be greatly appreciated!

Model Layer Information:

AI_I_0-1745159532196.png

Stm32 Anlyze Show Graph:

AI_I_1-1745160136547.png

 

1 reply

Julian E.
Technical Moderator
April 22, 2025

Hello @AI_I,

 

What is your issue exactly? you get an error using cubeAI or stedgeai core CLI?

Can you provide your model (in .zip) or source code please.

 

Have a good day,

Julian

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
AI_IAuthor
Associate II
April 22, 2025

Hello,

I'm new to CubeAI and would like to use it in one of my projects. I created a simple model (attached as a zip), but when running it on an STM32F4 series processor, I’m not getting any output. I’m not sure if my code is correct. I’d really appreciate it if I could get a basic output from this simple model.

Thank you in advance!

Julian E.
Technical Moderator
April 23, 2025

Hello @AI_I,

 

First, your model is correct.

 

Then, here is what I suggest you to do.

  1. Open STM32CubeMX
  2. Select your board
  3. Activate X Cube AI and select the systemPerformance template.
  4. Generate the code, build and flash
  5. Open tera term and you should see an output with some metrics.

For there, you can look at the code.

In the main() you will see a function called cubemx_ai_run or something close to that.

Use the debug option to understand what is being done. Basically, you just need to manage the inputs and outputs, X Cube AI does the rest.

 

You can also use the application template instead of the systemPerformace.

You will have to once again manage how you collect input and what you want to do with the outputs with functions template already in place.

 

Here is some documentation that should help you:

https://stedgeai-dc.st.com/assets/embedded-docs/embedded_client_api_legacy.html

The function names may be different, but the idea it the same.

 

Have a good day,

Julian

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.