Question
ReduceSum with operands type (SIGNED, 32 bit, C Size: 32 bits) is not supported
- February 11, 2025
- 1 reply
- 626 views
Hello!
I'm getting the error when I analyze an ONNX model using ST Edge AI Developer Cloud : NOT IMPLEMENTED: ReduceSum with operands type (SIGNED, 32 bit, C Size: 32 bits) is not supported. I have tried to convert the float32 data to float16, but it is not supported (TOOL ERROR: Unsupported elem type FLOAT16 for tensor Cast_1_output_0). The model was attached below. The model was generated in Pytorch, and the MCU was STM32H753VIT6. I'd like to know if anyone has had this problem and how it was resolved?
I would appreciate it if anyone could help to figure out what could be the problem. I attach my model below in case someone can help me. Thanks in advance. Regards!